2/6/2023 1:01 PM | |
Joined: 7/19/2022 Last visit: 5/9/2024 Posts: 358 Rating: (61) |
Hi fabioga66, WinCC stores the data in an SQL database. If you want to make sure that these files are not lost in case of PC corruption, you can, for example, make a copy of the files in the "ArchiveManager" folder of the WinCC project. The copy should always be made with the Runtime stopped.
|
If this Information really helps, you could use the Rate function |
|
2/7/2023 12:41 PM | |
Joined: 7/19/2022 Last visit: 5/9/2024 Posts: 358 Rating: (61) |
Hello fabioga66, I don't know if there is a software package to do what you are looking for, but maybe by running the following FAQ script every X amount of time you can copy those files to another folder: |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
2/10/2023 4:43 PM | |
Joined: 7/19/2022 Last visit: 5/9/2024 Posts: 358 Rating: (61) |
Hello again fabioga66, I have recently seen the existence of the tool "Copy WinCC Project": How do you backup/copy WinCC projects while WinCC Runtime is running? Delivery release Copy Project V6.5 This tool allows to make a copy of the whole project (including data base) during the Runtime. Here is the link to the mall: |
Last edited by: JBS98 at: 02/10/2023 16:44:12If this Information really helps, you could use the Rate function |
|
Follow us on