3/17/2023 11:44 PM | |
Joined: 3/9/2023 Last visit: 3/29/2023 Posts: 1 Rating: (0) |
Hi fredjoe Trying to establish if the Siemens LMQTTClient block actually works straight out of the box or not for communication with Azure. Yours seems to be only message that suggests it works without the user having to create something custom as per ThaiKibosh. I can’t actually see a release of the block for 3/9/2021 but there was a recent update in 2023. In any case I encounter the same 80C5 issue as most others. Can you please confirm? I only need to publish. The block seems to work on the same LAN without certificates but seems to fail for me when using QDN/DNS and certificates.
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/20/2023 09:31:12New subject after splitting |
|
3/20/2023 2:04 PM | |
Joined: 8/3/2009 Last visit: 4/26/2024 Posts: 12869 Rating: (1641) |
Hello https://support.industry.siemens.com/cs/de/en/view/109772284 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on