3/22/2023 7:08 PM | |
Joined: 9/1/2016 Last visit: 5/8/2024 Posts: 18 Rating: (0) |
Hi, I need to know if SmartClient is compatible on Windows 10 IoT Enterprise. Thanks a lot! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/31/2023 10:35:07New subject after splitting |
|
3/23/2023 7:17 AM | |
Joined: 8/3/2009 Last visit: 5/10/2024 Posts: 12924 Rating: (1646) |
Hello Yes I would say the latest Versions of SmartClient Exe should work with Windows 10. the application comes with the installation of TIA Portal, so if the compatibility of the corresponding TIA Version is OK then also the SmartClient should work. You can download here and give it a try. https://support.industry.siemens.com/cs/de/en/view/109482434 Bye Murof |
Last edited by: Murof at: 03/23/2023 07:19:02If this Information really helps, you could use the Rate function |
|
Follow us on