2/2/2024 12:54 AM | |
Joined: 1/25/2024 Last visit: 2/18/2024 Posts: 15 Rating: (0) |
This link is OK but for a rookies is to complicate, is there a list or table to see the LOGO! family compatibility? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 02/02/2024 12:18:11New subject after splitting |
|
2/2/2024 2:32 AM | |
Joined: 12/18/2014 Last visit: 4/27/2024 Posts: 32895 Rating: (4066)
|
No. But I think you don't want to work with older LOGO!s then the LOGO! 0BA8. Older LOGO!s 0BA0 - 0BA3 can't work with expansions module. Older LOGO!s 0BA4 - 0BA7 can work with expansions module if the article number of the expansions module ends with 0BA0 or 0BA1. Older LOGO!s 0BA4 - 0BA7 can't work with expansions module if the article number of the expansions module ends with 0BA2. 0BA8 LOGO!s are not compatible with expansions module if the article number of the expansions module ends with 0BA0 or 0BA1. 0BA8 LOGO!s are only compatible with expansions module if the article number of the expansions module ends with 0BA2. In attachment a small history of all 0BA8 LOGO!s. AttachmentVersions of 0BA8.txt (163 Downloads) |
Last edited by: ixo65 at: 02/02/2024 02:34:47 |
|
Follow us on