12/18/2012 2:33 PM | |
Joined: 9/27/2006 Last visit: 9/28/2024 Posts: 12283 Rating: (2685) |
Hello Rajkiran; I have no doubt that you can setup such a configuration. Here is some information available on the subject. From an older manual (from 1999, oldie but still goodie!) WinCC Option Client-Server Practical and Theoretical Limits in the Implementation of Client/Server: - Theoretically, due to software-technical limitations, WinCC can accommodate a maximum of 64 nodes (63 WinCC clients, 1 WinCC server) in one project. - Actually, however, the type and implementation of the process communication selected for the WinCC server is of great significance for a realistic number of WinCC clients. The system can be implemented with up to 8 WinCC clients. From a newer version, 2009, taking into account the evolution of network and computercapacities and WinCC itself: WinCC: Configurations Possible numbers of clients and servers Different quantity structures can be realized according to the type and number of client types used. Mixed systems are possible, meaning the parallel use of clients and WebClients within one client/server system.If you only use clients, in a WinCC network up to 32 parallel clients can access a server. One client can access up to 12 servers in runtime. A maximum of 24 servers can be implemented in the form of 12 redundant server pairs. When using WebClients, the limit is up to 51 clients (1 client and 50 WebClients). In such a system a maximum of 24 servers in the form of 12 redundant server pairs can be used. Hope this helps, Daniel Chartier |
12/18/2012 2:45 PM | |
Joined: 8/18/2009 Last visit: 6/17/2024 Posts: 548 Rating: (33) |
Deardchartier, I have serched in wincc doc.(attached). There is given Max. 3 clients. is it correct... means not possible 1server & 6 client. Please reply
|
Rajkiran Patil |
|
4/10/2024 5:46 AM | |
Joined: 4/14/2018 Last visit: 9/24/2024 Posts: 47 Rating: (1) |
For latest reference, You can visit the information center Wincc for more details on software requirements, in this link |
|
|