4/15/2024 9:25 AM | |
Joined: 1/22/2009 Last visit: 10/15/2024 Posts: 116 Rating: (17) |
Hello, please check the following FAQ: What should you watch out for when downloading from the WinCC/PCS 7 Engineering Station to the Operator Station (ES-OS download)? https://support.industry.siemens.com/cs/de/en/view/59216666 I would recommend to set this Services to Automatic start.Next please check that the Windows feature "Network Discovery" is turned on, on both PC's. You will find this Setting, in the "advanced sharing settings" in the "Network and Sharing Center". Please be reminded, that the following Windows Services have to be started to activate this feature: => DNS-Client => Function Discovery Resource Publication => SSDP Discovery => UPnP Device Host BR Fess |
Last edited by: Fess at: 04/15/2024 09:25:48Last edited by: The Helping Hand at: 04/15/2024 13:19:09Link optimized |
|
Follow us on