工业业务领域支持中心
Technical Forum
5/24/2024 9:49 AM | |
Joined: 5/24/2024 Last visit: 5/24/2024 Posts: 2 Rating: (0) |
Hi all, i'm a programmer from Volvo Cars Ghent and I have a question about STEP 7. Our PLC program is running on a server in the factory together with the WinCCViewerRT. We use thin client to connect to the server( see picture) to make changes to HMI. the Problem is that the server adress changes fromhttp://gensvw1212.gen.volvocars.nett ohttp://Localautomatically after a period of time. Is there a way to fix this in the settings that the server address is fixed ? Big thanks in advance!!! |
Follow us on