6/17/2024 3:42 PM | |
Joined: 2/17/2020 Last visit: 10/30/2024 Posts: 1104 Rating: (200) |
Hi, WinCC V7.5 SP2 is released for Windows 11 Pro 23H2 as of software Update 16 (link), so the base installation should be able to finish. Is this a new system or did you already have some software (perhaps another instance of SQL Server) installed previously? If it is a new system, I would recommend reinstalling the operating system (please do not use images or restore points). Then, set up the system and assign a unique computer name before installing WinCC (changing the computer name after installing WinCC will cause serious problems and require a new installation). Finally, start the WinCC installation. I really hope this helps! |
A rating will be well appreciated. |
|
This contribution was helpful to1 thankful Users |
6/19/2024 5:24 AM | |
Joined: 10/3/2010 Last visit: 10/31/2024 Posts: 1563 Rating: (192) |
On systems running Windows 11, some new storage devices and device drivers exposes a disk sector size greater than the SQL supported 4-KB sector size. When this occurs, SQL Server will be unable to start/install due to the unsupported file system as SQL Server currently supports sector storage sizes of 512 bytes and 4 KB. First check this:
|
B r g d s , |
|
This contribution was helpful to2 thankful Users |
6/19/2024 8:28 AM | |
Joined: 6/8/2023 Last visit: 9/3/2024 Posts: 4 Rating: (0) |
Hi SteBo, That seemed to solve my problem, I was now able to install Wincc without any problem. Thank you very much! |
6/19/2024 10:04 AM | |
Joined: 10/3/2010 Last visit: 10/31/2024 Posts: 1563 Rating: (192) |
Thanks for letting us know! |
B r g d s , |
|
Follow us on