6/26/2024 9:18 AM | |
Joined: 8/3/2009 Last visit: 9/27/2024 Posts: 13803 Rating: (1742)
|
Hello vorapob Of course you can also connect to the S71500 PLC with WinCC and read the Tags from AS but you need to work at least one time with the SCADA Export Tool to get also the Certificate from the S71500 for the Secure HMI communication. If you do not use it the certificate will not be imported and the communication can not be established. And the basics you can find here: https://support.industry.siemens.com/cs/de/en/view/101908495 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on