9/11/2024 6:33 PM | |
Joined: 3/14/2008 Last visit: 9/26/2024 Posts: 2098 Rating: (938)
|
Hi, This means it's a license with no software attached. This license should be transferred to ALM on the OS server(s). It's a license for archiving 1500 tags. The amount of tags used in the project can be collected from the PCS7 license information (via right click of the multiproject in Simatic Manager). If you have two OS servers (redundant), you need to but the license two times. |
If I could help you, you can use the RATE button. Thank you. |
|
9/18/2024 2:17 AM | |
Joined: 11/20/2018 Last visit: 9/22/2024 Posts: 17 Rating: (0) |
Thank you, And what means with R-SW? R stand for redundant or Runtime? |
Last edited by: MH-KARAMI at: 09/18/2024 02:18:41 |
|
Follow us on