10/16/2024 8:41 AM | |
Posts: 3 Rating:
|
Dears, Fire alarm resistance cable (2*1.5mm2) copper , with ρ=12.1 ohm/km per conductor,the cable mentioned is used for fire alarm loop on XDLC Card , loop devices =200 device. please i want to calculate the maximum length of the loop that can cable withstand. ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 10/16/2024 09:09:09New subject after splitting |
|
10/16/2024 9:11 AM | |
Joined: 7/30/2024 Last visit: 9/18/2025 Posts: 962 Rating:
|
Closed because posted twice. The active topic can be found here: Loop Length Calculations For Cerebrus Pro MOdular system
Kind regards, Moderator_Lan |
Follow us on