3/28/2025 11:48 AM | |
Joined: 2/10/2023 Last visit: 9/15/2025 Posts: 6 Rating:
|
I am having problems with emails on LSC 8.4.1 and firmware 1.84.03. It will allow me to add *.com, however, not *.co.uk, is there a solution to this as it just says "Removed invalid or duplicate email address", see attachments. Also why does it need login credentials for port 25 legacy use, this port doesn't need credentials on our system? AttachmentLSC 8.4.1.zip (272 Downloads) |
3/28/2025 12:12 PM | |
Joined: 12/18/2014 Last visit: 9/20/2025 Posts: 36022 Rating:
|
No one in the forum will be able to help you. I assume the second dot in "*.co.uk" isn't allowed. I can only recommend that you to start a Support Request. |
This contribution was helpful to
1 thankful Users |
3/31/2025 11:41 AM | |
Joined: 12/18/2014 Last visit: 9/20/2025 Posts: 36022 Rating:
|
I think with the next firmware update (V1.84 04) ... |
This contribution was helpful to
1 thankful Users |
3/31/2025 12:29 PM | |
Joined: 12/13/2014 Last visit: 7/7/2025 Posts: 156 Rating:
|
Legendary german punctuality and accuracy in everything.. I myself thought it was an LSC error altogether. Btw, this same bug was even earlier, in 1.84.02 (my message, describing same issue, is latest in thread). |
Follow us on