3/23/2022 4:43 PM | |
Joined: 2/17/2020 Last visit: 9/22/2025 Posts: 1251 Rating:
|
Hi alextu, Please see the following link: "The service can be easily simplified through: - The device replacement without PC and engineering software via Backup/Restore using a USB stick". Phase-out: SITOP smart 24 V/2,5 A, 24 V/5 A, 24 V/10 A Apparently, you could use the backup as a restore in the new panel. |
A rating will be well appreciated. |
|
3/30/2022 10:19 AM | |
Joined: 8/3/2009 Last visit: 9/23/2025 Posts: 16473 Rating:
|
Hello Itafusna SITOP? did you use the wrong link? its because hte topic is about Multi Panel. I would say the Restore would make problems. I would transfer the Panale again with engineering project (WinCC flexible or TIA) Bye Murof |
If this Information really helps, you could use the Rate function |
|
4/4/2022 8:43 AM | |
Joined: 2/17/2020 Last visit: 9/22/2025 Posts: 1251 Rating:
|
Hi, Yes, Murof, thanks for notifying me. I must have copied the wrong link. Here is the right one, being a product change from 1st Gen to 2nd Gen HMI panels: Announcement of product phase-out for the 1st Generation Basic Panels |
A rating will be well appreciated. |
|
9/19/2025 11:18 AM | |
Joined: 8/3/2009 Last visit: 9/23/2025 Posts: 16473 Rating:
|
Hello Im not 100% sure but I think a Backup Restore should work because the changes were slightly only a bit of HW. It should be functional compatible: https://support.industry.siemens.com/cs/de/en/view/109486162 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on