9/10/2007 6:31 PM | |
Posts: 191 Rating: (58) |
Hi!! thisis a tricky one... please look at the attachment, it uses the logic ofa binary counter. Hope this helps!! ROSA AttachmentShift register.zip (822 Downloads) |
9/10/2007 11:29 PM | |
Joined: 1/5/2007 Last visit: 4/7/2023 Posts: 1690 Rating: (580) |
Hello, in the attachment you find a general solution to program - an edge triggert RS-Flip-Flop - an edge triggert D-Flip-Flop - a 3-bit shift register as an example for bilding a n-bit shift register build with D-Flip-Flops - a 3-bit ring register as an example for bilding a n-bit ring register (build with D-Flip-Flops and 2 to 1 Multiplexer). Two Exampleswith differend control inputs. Perhaps it isinteresting for you a link to two program solutions for - a counter with predefined value - a counter which can count values in the range -32767 to 32767 !!! Demo_Zähler_mit_definiertem_Wert_vorspannen.zip I hope this can help you! Best regards Betel AttachmentForum_3bit_shiftregister.zip (1324 Downloads) |
==> Meine TAG-Listen: "deut." |
|
9/11/2007 11:30 AM | |
Posts: 2 Rating: (0) |
Now I think to haveenough material to continue on my own. Thank everybody very much for your helps! |
Follow us on