12/5/2017 6:55 PM | |
Joined: 11/21/2007 Last visit: 7/25/2025 Posts: 2326 Rating:
|
Hello The SIMATIC M7-300/400 was a PC-compatible automation computer. It was designed as an enclosed modular system designed for SIMATIC S7 racks. One required STEP7 with optional M7 package for programming. M7 optional packages made it possible for you to use high-level programming languages such as C or C++ as well as graphic programming software such as CFC (Continuous Function Chart) . Here are some Manuals to give you an Idea for M7 : M7-300 Programmable Controller Hardware and Installation System Software for M7-300 and M7-400 Installation and Operation System Software for M7–300/400 Program Design Hope this helps Cheers Navnag |
Last edited by: Jen_Moderator at: 12/6/2017 10:16:34 AMInserted right links. There is no such thing as the last bug in a program |
|
This contribution was helpful to
1 thankful Users |
Follow us on