1/9/2021 6:58 AM | |
Posts: 8 Rating: (0) |
Hi, We have a winder application and we are using Parker Drive. I want to use G120. I have seen the article below but it requires a PLC. : https://support.industry.siemens.com/cs/ww/en/view/58565043 I know about speed control but I want to know about the commissioning of torque mode without PLC. I am commissioning with starter and set following parameters during commissioning P96=0 Expert Mode P1300=22 Control Type P15=12 Analog Set Point After commissioning, I can see Analog Input is set as speed setpoint (image attached) while Torque setpoint is blank (Image Attached) Do I have to replace the speed setpoint as torque setpoint or I have to provide one more analog input for torque setpoint. ------------------------------------------------------------------------------------------ Attachmentimage.zip (1115 Downloads) |
Last edited by: Jen_Moderator at: 01/11/2021 07:11:59New subject after splitting. Optimized link |
|
Follow us on