1/29/2023 12:10 PM | |
Joined: 7/21/2021 Last visit: 9/14/2023 Posts: 14 Rating: (0) |
Hi All, I have started to learn the simotion OOPS concept. For that, I am using a simotion D425-2PN CPU and tested a sample program with SIMOSIM. Now my question is, in the sample program, they declared the interface as an input Variable and passed the class's instance to that variable for calling the corresponding class methods. Now I want to monitor which class is passed to that variable, but online I couldn’t be able to see that class name… Thanks in advance AttachmentClass_Monitor.zip (364 Downloads) |
Follow us on