2/5/2023 11:58 AM | |
Joined: 2/5/2023 Last visit: 2/7/2023 Posts: 4 Rating: (0) |
How to connect an external touch screen to use it instead of the main touchscreen of KTP900 Basic… 6AV2123-2JB03-0AX0? |
2/7/2023 8:10 AM | |
Joined: 3/30/2020 Last visit: 4/25/2024 Posts: 4443 Rating: (928) |
Perhaps a license is not needed: |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
This contribution was helpful to1 thankful Users |
2/7/2023 1:44 PM | |
Joined: 8/3/2009 Last visit: 4/25/2024 Posts: 12869 Rating: (1640)
|
Hello MHMah SmartServer is a VNC Server that can run on the Panel. It will not replace the panel. Here you can remote control the Panel from outside. If your Screen is damaged you should send it to repair center: https://support.industry.siemens.com/cs/ww/en/view/22639376 you can try the smartServer also without license. Since V17/V17 Image you do not need a Smart Server licenese any more, its included also with Basic Panels 2nde Gen. Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
Follow us on