2/1/2023 2:01 PM | |
Joined: 1/21/2013 Last visit: 5/5/2024 Posts: 2742 Rating: (444) |
Hi JacopoPodavini,
the 'Press' event is suitable for this purpose, the default would be 'Click left mouse button'. Both event types are for mouse and touch input. The 'Press' event is also triggered by keyboard input. The 'Press key' event is for keyboard events only! See 'Basics on the events'. So this is unlikely to be the cause of the behavior you are experiencing. We would need more information about the software you are using. Do you have the latest update installed? Is the latest V16 image version being used (you can also try a newer image version)? Is it possible to update your TIA Portal to a newer version? Kind regards |