3/11/2024 7:49 PM | |
Joined: 2/4/2024 Last visit: 6/2/2024 Posts: 7 Rating: (0) |
Goodnight I have a problem with a LAGUN CNC manufactured in 1997 equipped with SIMODRIVE 611. The following errors appear on the display of the Main Spindle Module: F09 and F19, according to the specific manual for the encoder and motor temperature probe, respectively. I checked that the probe is at 600 ohms at 20ºC and that the ERN 1387 encoder is OK. The connecting cable and plugs are OK. It's probably a problem with the control boards. So I have questions about the specific boards of the 1P control unit 6SN1121-0BA11-0AA0 E-stand version A. This unit is equipped with subcards: T-J76822F0, T-J83592F0 T-J84162F0, fitted in slots X12, X13, X16, respectively. Which board is responsible for controlling the encoder and motor temperature? Is the sequence of slots X12, X13, X16 correct? Where can I find these cards? Can anyone shed some light? ------------------------------------------------------------------------------------------ |
Last edited by: Fertec.Fertec at: 03/11/2024 20:46:46Last edited by: Fertec.Fertec at: 03/11/2024 20:50:57Last edited by: Fertec.Fertec at: 03/11/2024 20:51:42Last edited by: The Helping Hand at: 03/12/2024 12:36:17New subject after splitting |
|
3/12/2024 12:40 PM | |
Joined: 8/21/2014 Last visit: 6/17/2024 Posts: 970 Rating: (13) |
Closed cause question posted twice. The second thread with the subject Simodrive 611 Error F09 and F19 is published within the conference SIMODRIVE Converter system Best regards, |
My Forum is the place to personalize your profile, |
|
Follow us on