3/20/2024 2:20 PM | |
Joined: 9/27/2006 Last visit: 4/26/2024 Posts: 12257 Rating: (2665) |
Hello; E238 and E239 are not error messages generated by the S7-200 PLC. For confirmation, open the S7-200 System Manual, Appendix C, Error Codes: https://support.industry.siemens.com/cs/ca/en/view/1109582 It must be from the SPUHL C313 spring winding machine. I suggest you start by looking up the user manual for the machine, or by contact support from SPUHL. From the web, this is contact information for Spuhl Gmbh: Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
Follow us on