10/31/2024 3:35 PM | |
Joined: 5/6/2022 Last visit: 9/15/2025 Posts: 589 Rating:
|
Hi M.Radovic, Yes, Siemens offers panels that are well-suited for humid environments where operators might need to touch the panel with wet hands frequently. Specifically, the SIMATIC HMI TP700 Comfort INOX PCT and other INOX panels with glass fronts are designed for such challenging conditions. These panels have a high degree of protection (IP69K and IP66K), making them resistant to water and suitable for environments requiring frequent cleaning or exposure to moisture. They also feature high chemical resistance, which is beneficial in environments where disinfectants are used (Product note: Delivery release for INOX Comfort Panel TP700 with glass front). Additionally, the SIPLUS HMI Comfort Panels Outdoor are designed to withstand extreme conditions, including high humidity and direct sunlight. These panels are robust and feature a bonded display to prevent moisture infiltration, making them suitable for outdoor and harsh environments (SIPLUS Comfort Panels Outdoor). Hope this information can be helpful. Best regards!
|
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
Follow us on