(0)| 11/19/2024 8:46 AM | |
|
Joined: 8/3/2009 Last visit: 1/9/2026 Posts: 16629 Rating:
|
Hello lovol110 If you want to access a network share you have two options. 1.) Use networkshare directly -> then you have to use SMB V1.0 (and this is nowadays often blocked by IT) Then you can access the network share directly form the HMI by \\Servename\sharename 2.)Option+ Manager -> you do not have to use SMB for filetransfer, it works via Webserver The Option+Manager SW has to run on the PC Everything is explained here: https://support.industry.siemens.com/cs/ww/en/view/92346478 Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
Follow us on