(0)| 5/24/2020 3:11 PM | |
|
Joined: 9/27/2006 Last visit: 12/29/2025 Posts: 12477 Rating:
|
Hello HEM; If you have not yet selected to final model of your KTP700, I would like to point out the following KTP700 Basic DP unit, which comes with an integrated Profibus-DP connection that you can easily set up with your ABB controller, as per the original commissioning. See the screenshot below. The other model is the KTP700 Basic, which comes with an integrated Profinet port: 6AV2123-2GB03-0AX0. Here is a link to the HMI Basic Devices (2nd Generation) manual, which discusses this DP variation and others, it will show you can use various alternat communications networks to connect to the HMI, among them Modbus RTU and Profinet. https://support.industry.siemens.com/cs/ww/en/view/90114350 Hope this helps, |
Last edited by: dchartier at: 05/24/2020 16:46:12 |
|
This contribution was helpful to
|
|
| 12/15/2025 8:32 AM | |
|
Joined: 10/9/2019 Last visit: 12/15/2025 Posts: 1 Rating:
|
Could you also share that information and the example program project? |
Follow us on