(3)| 5/26/2014 6:54 AM | |
|
Joined: 6/8/2013 Last visit: 12/15/2025 Posts: 160 Rating:
|
hi, What is the diff. between BACNET ms/tp and ip protocol ? ie. speed , distance Thanks
A. G. Naphade |
| 5/26/2014 9:50 AM | |
|
Posts: 12 Rating:
|
BACnet ms/tp is a datalink link layer protocol based on EIA-485, cable length depends on used speed, up to 76800 bits per seoconds it is 1200m. For wiring, termination resistors and grounding see attachment. BACnet/P stands for BACnet over Ethernet 802.3., Typical speed is 100 mega bits per seconds. cable length depends ob cable type, typically 100 m AttachmentD:\Downloads\BACnet_Doku\Auszug_Standard_MS_TP.pdf (1666 Downloads) |
This contribution was helpful to
|
|
| 5/30/2014 6:08 PM | |
|
Posts: 59 Rating:
|
Thank You For PDF Attachment Its USefull FOr US REgard Shailesh |
Follow us on