3/20/2013 6:47 PM | |
Posts: 14 Rating: (0) |
SIR I am also facing the same problem ,and my case R 47 word message is 3 please can you advice on this please . with regards vikas prakash singh |
3/21/2013 3:12 AM | |
Joined: 8/25/2006 Last visit: 5/31/2024 Posts: 2206 Rating: (278) |
Hello. Look at themanual, chapter 10. F005, fault value 3: Delay time according to P089 elapsed in state o5.0 Wait until IField act (K0265) > 50% of the instantaneous field current setpoint K0268 [as of SW 1.9, can be altered bymeans of P396] and until "I Field extern > I f min" (see P265). |
4/24/2013 6:07 PM | |
Joined: 8/25/2006 Last visit: 5/31/2024 Posts: 2206 Rating: (278) |
Hello. What is the value of P082, when F005 occurs? Check also connections of field supply (AC and DC side).
|
4/29/2013 2:53 PM | |
Joined: 8/25/2006 Last visit: 5/31/2024 Posts: 2206 Rating: (278) |
Hello. Previously you have wrote:
Please specify the complete order number of the drive. Have you followed step-by-step start-up procedure described in themanual(section 7.5), especially did you reduce rated converter armature and field currents (page 7/19), as you try to work on a 65A motor with 850A converter.
|
4/29/2013 3:49 PM | |
Posts: 14 Rating: (0) |
Dear sir thank you for your reply i am working on drive, type:D520/850 Merg -GeGE4V62-4A 6RA 2487-4GV62-0 with regards Vikas Prakash singh |
4/30/2013 5:59 AM | |
Joined: 8/25/2006 Last visit: 5/31/2024 Posts: 2206 Rating: (278) |
Hello. So, you have 850A armature/30A field drive and want to run 60A armature/2.8A field motor. Refer to chapter 6.6 of themanualabout load and shunt resistors for armature/field curcuits, which may be removed for reducing rated converter armature/field currents. Also don't forget to reduce this currents in parameters P072, P073, as described in chapter 7.5.
|
This contribution was helpful to1 thankful Users |
1/17/2017 3:25 PM | |
Posts: 1 Rating: (0) |
Please chek cable conection ot terminal block,mcb,nfb. Maybe blow/heat Thnks Dani |
5/30/2017 5:59 AM | |
Joined: 8/25/2006 Last visit: 5/31/2024 Posts: 2206 Rating: (278)
|
Hello. Look here. |
9/15/2017 9:00 PM | |
Posts: 3 Rating: (0) |
We face the same problem with the same drive and was solved by reducing set point in p102 |
Follow us on