3/4/2014 4:51 AM | |
Joined: 5/12/2006 Last visit: 9/2/2025 Posts: 22709 Rating:
|
Hello, HF12 is a full setup and not only a HF delta-setup, so you must order this version or load it via PridaNet. Further Information for HF12 you will find here. Regards Christoph |
This contribution was helpful to
1 thankful Users |
3/10/2015 11:34 AM | |
Posts: 1 Rating:
|
Hello Mr.Christoph Hill, which version of SIMOTION SCOUT is required for communicating the ""Simotion D4X5-2 V4.4 HF1 + SINAMICS 4.7 HF1"". Currently i have scout 4.3 sp1 hf9. this version is able to detect the NODE but not the device. Is there any SSP available for this version? Regards, Harshavardhan Reddy |
9/6/2022 9:34 PM | |
Joined: 12/13/2015 Last visit: 5/7/2024 Posts: 22 Rating:
|
dear's, i need the link to download the simotion scout 4.3 HF1 |
9/7/2022 11:36 AM | |
Joined: 1/4/2013 Last visit: 8/13/2025 Posts: 1186 Rating:
|
Hello HF1 does not exists anymore. Download the last 4.3 SP1 Hotfix, it is FULLY compatible : Here |
Last edited by: Jen_Moderator at: 09/21/2022 09:12:33Link optimized. Searching for Siemens used/new equipments ? |
|
Follow us on