8/14/2022 2:45 PM | |
Joined: 1/9/2019 Last visit: 3/22/2025 Posts: 88 Rating:
|
HI, I have one simotion d425 system, the system was fine and working with CF card v5.2, the system controls 4 axes and the old CF card was 6AU1400-2PA22-0AA0-Z=44 for testing we power off the simotion and remove CF CARD and then insert new one with firmware v4.3 (6AU1400-2PA22-0AA0-Z) as you can see in fig "CF1" after power-on all led's on d425 was red and the ready LED blinking red and orange . and the display shows .8 as you can see in fig "led", So I think maybe the firmware of CF card is the problem and I upgrade it to version 5.3 from siemens site, but the problem didn't solved. the other problem is that I can not connect to this d425 any more (the version of simotion is 5.3). I changed the CF card with another one with z=43 but the problem was the same. can any one help me on that? AttachmentDesktop.zip (535 Downloads) |
Last edited by: mpakravanan at: 08/14/2022 14:49:50 |
|
8/15/2022 7:31 AM | |
Joined: 5/12/2006 Last visit: 9/2/2025 Posts: 22709 Rating:
|
and do it work with the first CF you have removed? |
This contribution was helpful to
1 thankful Users |
8/15/2022 4:12 PM | |
Joined: 10/11/2006 Last visit: 9/8/2025 Posts: 6039 Rating:
|
hello additional Information about LED : https://support.industry.siemens.com/cs/ww/en/view/109781516 State 8 indicates a problem with the battery/fan module. (please have a look if module is present) |
With best regards, |
|
This contribution was helpful to
1 thankful Users |
Follow us on