4/26/2023 9:59 AM | |
Joined: 3/2/2007 Last visit: 9/9/2025 Posts: 990 Rating:
|
Kindly, during the installation of Scout Tia software, we got some errors. Check attached and below. Simotion Scout Tia v5.4 sp3 (Tia Portal v17) An error occurred during setup. Details are listed in the setup report. Files for setup analysis (for customer support). Creating config files failed! Please check the log files for details. mkcfgdb???_Log.txt hwkatimport???_Log.txt Installation errors occurred! Please check the log file. Install_Scout_Tia_Classic_5.4.txt AttachmentSIA_SCOUT_TIA_V5_4@23-04-26_11-12-17_summary.log.txt (575 Downloads) |
... thank you ... |
|
4/26/2023 10:04 AM | |
Joined: 5/12/2006 Last visit: 9/2/2025 Posts: 22709 Rating:
|
and have you check the logfiles which are named? The one attached ist none of them and give no error details |
4/26/2023 10:39 AM | |
Joined: 3/2/2007 Last visit: 9/9/2025 Posts: 990 Rating:
|
I found these errors, as in the attached. SIA_SCOUT_TIA_V5_4@23-04-26_11-12-17_summary.log ERROR AdsWorkerForeignExe::GetInstallResult(): - -1: assuming unknown error, because return value is not in OK-list which is only defined. Please check the corresponding log file for more detailed information FAIL! SetupUnit (MKCFGDB) Failed Foreign AddLocal Intermediate ExitCode after execution queue : 1603 - Exit code means: Installation failed (InstallFailure) Errors: 1 C:\ProgramData\Siemens\Automation\logfiles\Setup\mkcfgdb???_Log.txt install_request -i -TO BES_IT_TOSDGen -y ssp_simotion_int_v5_2_3\V5.2.3\u7boIS201011tx.ini failed! u7bt05ax.exe -scan u7setup failed! Error: Creating config-files for UMCInstallation failed C:\ProgramData\Siemens\Automation\logfiles\Setup\hwkatimport???_Log.txt could not find this file in the folder. C:\ProgramData\Siemens\Automation\logfiles\Setup\Install_Scout_Tia_Classic_5.4.txt ERROR: Function CallMkcfgdb, creating config files failed Attachmentmkcfgdbpe.bat_042623_112938_Log.txt (525 Downloads) |
Last edited by: Ziemens at: 04/26/2023 10:40:35Last edited by: Ziemens at: 04/26/2023 10:41:10... thank you ... |
|
Follow us on