5/7/2016 5:48 AM |
|
Joined: 12/18/2014 Last visit: 9/12/2025 Posts: 35955 Rating:
|
Take a look to these links, perhaps this help you: https://ssl.arcor-secure.de/systeme-lauer.de/forum/pcs_f.htm |
5/7/2016 6:17 AM | |
Posts: 153 Rating:
|
Hi ixo65 I have all of them, but i was confused because i had never use lauer hmi before i dont know "The memory address of S5 connect with Lauer is fix (example: if vobi=50, address connect with F1..F20 button, value display... is fix or not ) or can configure with different memmory address like new siemens HMI (example: F1: M100.0, F2: M20.7,F3: M40.4...)". thank you |
5/7/2016 8:02 AM | |
Joined: 11/21/2007 Last visit: 7/25/2025 Posts: 2326 Rating:
|
Hello These assignments are in a System Data area which is defined using pcspro software. |
Last edited by: Navnag at: 5/7/2016 8:03:21 AMThere is no such thing as the last bug in a program |
|
This contribution was helpful to
3 thankful Users |
4/15/2025 6:50 AM | |
Joined: 11/17/2023 Last visit: 6/24/2025 Posts: 1 Rating:
|
Hi ixo65 Is it possible to make the documentation links available again? They are no longer accessible. thanks |
Follow us on