8/25/2025 12:56 PM | |
Joined: 9/13/2012 Last visit: 8/26/2025 Posts: 27 Rating:
|
Dears. I have issue with our Simotin D425.Today I get part of the line stopped by the simotion D425. All 4 axixs controlers had errors led on as well as SMC30 controlers . I have old project unfortuanetly from 2016 and I had 2 or 3 scouts updates so I cannot connect with full compatibility but at least I could do Diagnostitic buffer check. Here is list of errors from one stop. Any advices how to finad the reason for such a behaviour ? It looks like some general error because 9 modules get error. CPU and power supply seems to be fine, only RDY led on D425 lights in red . I found some manual and description is : Device 1 0x8000h DP: Life-sign of drive has malfunctioned or failed Device 2 DP: 0x8000h Life-sign of encoder has malfunctioned or failed. It looks as problem with profibus … Strange because comunication between the modules is DriveCliq Should i consider also Drivecliq or concentrate on Probibus ? Attachment0825_Log.txt (4 Downloads) |
Last edited by: Moderator_Lan at: 08/25/2025 13:43:53Log attached |
|
Follow us on