8/5/2009 8:05 PM | |
Posts: 2 Rating:
|
hello: I have a doubt with a spare for magnetic flow meter, I bought a sensor prom with part number: FDK-085U1005,but when I received it the part number indicated is: FDK-085U0205. I have asked to the salesman in Siemens Mexico, but the answer is so slow, any body can answer me if is the same spare but the part number has changed? Is there some information in order to support this change? Could I get a copy? AttachmentP8030759.zip (727 Downloads) |
8/6/2009 8:24 AM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Hello, FDK-085U1005 • 2 kB (for MAG 5000/6000/ MAG 6000 I) (Sensor code and serial numbers must be specified on order). And basically if you put another type you'll receive error F62 - SENSORPROM® ID Replace (The SENSORPROM® unit ID does not comply with the product ID. The SENSORPROM® unit is from another type of product SITRANS FC, SITRANS FUS etc.). Take a look at SITRANS F flowmetersThere you'll find a lot of info about sensorprom modules and accessoaries with their order numbers. Unforunately the number that you'll received doesn't exist. I was also suprised you didn't received answer from Siemens about this number.Hope I was helpful a little. Best regards, Hristo Mihalev |
8/6/2009 6:03 PM | |
Posts: 2 Rating:
|
Umencho: thanks a lot for your help, we are going to test this sensorprom. the service in Siemens Mexico is bad, the answer was: "is the only sensorprom we have for these products, the number indicated doesn´t matter, are just for our control" if you can see the photographs the number impresed in the sensorprom is similar to the order number indicated in the literature for the sersorprom required. nobody knows this number, but if my customer see it, hethinks this is the part number and if this doesn´t match with the required hewill not accept this product. anyway I value your answer. Mario Chimal Briseño AttachmentP8030759.zip (635 Downloads) |
Follow us on