4/14/2010 9:33 PM | |
Posts: 116 Rating:
|
Hi, see http://support.automation.siemens.com/WW/view/en/25508507 Chapter 9: Motor reactors reduce the voltage stress on the motor windings by reducing the voltagegradients at the motor terminals that occur when motors are fed from drive converters. At thesame time, the capacitive re-charging currents that additionally load the output of the Power Module when longer motor cables are used are simultaneously reduced. |
Last edited by: Jerry at: 4/14/2010 9:52 PM |
|
Follow us on