5/18/2010 4:53 AM | |
Joined: 1/17/2006 Last visit: 7/14/2025 Posts: 554 Rating:
|
Hello Jerry, Thanks for your help and for the good tips and link! Today I tried to do a simple application using MCC and LAD/FBD units andinboth casesI could enable the drive (_mc_power), stop (_mc_stop)and start movement(_mc_movevelocity) of the MM440 axis. But, I could not change parametersas ramp-up time (p1120) and ramp-down time (p1121) in seconds directly, only changing the Acceleration and Desaceleration in "Dynamics" tab/block. I also tried to write in drive parameter (p1120/p1121) using the _writedriveparameter block from Drives>SIMOVERT in Command Library, but I had difficulty to fill out the parameters in the block. Is this theright way to follow ? Could you please help me with this issue as well ? Best regards, Berg Splitted from MM4 and Simotion SCOUT 4.1.4.1. |
Last edited by: O_Moderator at: 5/18/2010 1:12 PMnew subject after splitting Last edited by: Berg at: 5/18/2010 4:56 AM |
|
Follow us on