6/4/2010 10:04 AM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Hello, The messages "Rack error", "Module error" and "Periphery access error" are no longer generated by the Siwa_U component itself but by the components created with the PCS7 driver wizard. Look for more (plus example) at SIWAREX U Library for PCS 7 Best regards, Hristo Mihalev |
6/4/2010 11:38 AM | |
Joined: 9/5/2007 Last visit: 6/5/2025 Posts: 24 Rating:
|
Thanks for the reply.We have seen the "Manual_U_PCS7_60_en.pdf", where it is mentioned that the component itself will generate the module driver.But after compilation it is showing the warning that no hardware found for this base address of the configure Siwarex module.So what will be possible remedy of the same? Please guide us?
AttachmentMDI5ODY1MTk5MzUzMzQ2ODUzAAAA_10183075_2_inter_WW_2010-02-02.pdf (462 Downloads) |
Last edited by: DESH at: 6/6/2010 1:24 PMWe have purchased the Siwarex U module (MLFB No. 7MH4950-2AA01) and the SIWAREX U PCS7 configuration package V6.x (also suitable for V7.0 and V7.1) ,which is applicable to 7MH4601-2AA01 and 7MH4601-2BA01 : 7MH4683-3BA64, as per the enclosed doccuments. Not only that we have observed that the SIWAREX U PCS7 configuration package V7.0 and V7.1 (applicable to 7MH4950-1AA01 and 7MH4950-2AA01): 7MH4950-3AK61. So, can anybody clarify us that whether our procure package (7MH4683-3BA64) will be compatible with above module (7MH4950-2AA01) or not? |
|
Follow us on