1/7/2015 8:46 AM | |
Joined: 8/10/2012 Last visit: 8/15/2025 Posts: 14 Rating:
|
HI I have V4.1 of Simotion D & TP CAM V4.1.1.15 |
1/7/2015 10:08 AM | |
Joined: 8/10/2012 Last visit: 8/15/2025 Posts: 14 Rating:
|
Hi I have V4.1.5.15 |
1/7/2015 11:01 AM | |
Joined: 8/10/2012 Last visit: 8/15/2025 Posts: 14 Rating:
|
HI Ok. From where I will get TP V 4.1.5.15? |
1/7/2015 11:42 AM | |
Joined: 8/10/2012 Last visit: 8/15/2025 Posts: 14 Rating:
|
hi, I have tried with TP V 4.1.5.15 also, but it gives same error I have order no: 6AU1 435-0AA00-0AA1 |
1/7/2015 11:45 AM | |
Joined: 5/12/2006 Last visit: 9/2/2025 Posts: 22709 Rating:
|
and which messages are in the diagnostic Log of the simotion? |
11/18/2016 8:19 AM | ||||||
Posts: 6 Rating:
|
I have also same error with Simotion D410-2
Can you help me about TP error? |
|||||
11/18/2016 8:50 AM | |
Posts: 6 Rating:
|
I am sending all info about my scout version and device version in zip.Could you look please?I connect to the device via ethernet.
AttachmentSIMOTION_D410_2.zip (508 Downloads) |
Last edited by: ismetbjk at: 11/18/2016 8:53:27 AM |
|
11/18/2016 9:16 AM | |
Joined: 5/12/2006 Last visit: 9/2/2025 Posts: 22709 Rating:
|
diagnostic buffer? from the error in the download windows it looks that something is wrong with the version ot the TP, this can be a defective installation of scout. |
11/18/2016 10:11 AM | |
Posts: 6 Rating:
|
Also how can I fix this problem? I am sending diag buffer in attachment.
AttachmentSIMOTION_D410_2.zip (464 Downloads) |
11/18/2016 10:23 AM | |
Joined: 5/12/2006 Last visit: 9/2/2025 Posts: 22709 Rating:
|
Hi, is there any project data on the D410? Clean all data and then try to download again. Or download the project offline to the CF and then power up the system with the project on the CF Card. Offline Download can be done in the conterxt menu of the PLC (Load to File system) Regards Christoph |
Follow us on