7/28/2021 11:17 AM | |
Joined: 3/11/2019 Last visit: 9/6/2024 Posts: 1569 Rating: (288) |
Hi HIM61, as Towome already mentioned, V2.0.0 can only be installed from product release (ES-Version) 05. The version can be found in the online diagnostics of the module (hardware), or printed on the module. Therefore, the following FAQ can be helpful. How do you determine the release status of a SIMATIC device or module?
regards sancruz |
Feedback appreciated, please rate |
|
This contribution was helpful to3 thankful Users |
7/29/2021 10:50 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1054)
|
hi HIM61, no, you have state 4! anyway, you can update your FW to 1.0.4. Firmware Update for ET 200SP F-DQ 4xDC 24V/2AWhat TIA-version do you use? In older TIA-versions the module is only projectable with GSDML. you can find it here: PROFINET GSD files: I/O - ET 200SPBut you can also project it as predecessor with FW1.0.x hope this helps, regards, |
Last edited by: mopS04 at: 07/29/2021 10:54:53FCK WAR! |
|
This contribution was helpful to1 thankful Users |
Follow us on