9/9/2021 1:32 PM | |
Joined: 5/12/2006 Last visit: 8/13/2024 Posts: 22342 Rating:
|
which version you need? which error you get exactly(Scrren)? |
9/9/2021 1:57 PM | |
Joined: 3/11/2019 Last visit: 8/13/2024 Posts: 1552 Rating:
|
Dear P.Kow, the firmware is included in the following GSD. After installation, the device can be found in catalog folder "Other field devices" (other folder than the device from integrated hw catalog). But the newer firmware in the real hardware is compatible if you use V4.1 in the hw-config. The "Additional Information" is only an information. So for the error, there must be a different reason. For example, if the wrong baseunit is configured. PROFINET GSD files: I/O - ET 200SPregards sancruz |
Last edited by: sancruz at: 09/09/2021 13:58:44Feedback appreciated, please rate |
|
Follow us on