1/10/2022 11:51 AM | |
Joined: 5/30/2016 Last visit: 12/12/2023 Posts: 31 Rating:
|
Hello. Siemens PLC1516F stops, and i cannot find what is bad with the safety modules or program. I attached .zip with two photos of plc diagnostic error messages, maybe anyone have ideas ? Found this one, trying to figure it out : https://support.industry.siemens.com/cs/ww/en/view/19183712 AttachmentPLC_STOP.zip (88 Downloads) |
Last edited by: DariusB at: 01/10/2022 12:10:55Last edited by: Jen_Moderator at: 01/10/2022 14:04:08Optimized link. |
|
1/14/2022 8:03 AM | |
Joined: 10/10/2005 Last visit: 4/18/2024 Posts: 1917 Rating:
|
Hello DariusB, if the FAQ 19183712 is not successful, then update your soft- and hardware. Which STEP 7 version have installed? I recommend to install the last update of the STEP 7 version. Example for STEP 7 (TIA Portal) V17 I recommend to install the update 2. See in this case the link: Updates for STEP 7 V17, S7-PLCSIM V17 and WinCC V17 I recommend also to update the firmware version of the S7-1500F CPU. The firmware version V2.9 is available in STEP 7 (TIA Portal) V17. After updates compile the hard- and software complete with the two menu instructions:
Repeat the download again. With best regards |
Follow us on