1/18/2022 6:38 PM | |
Joined: 11/8/2017 Last visit: 9/27/2024 Posts: 337 Rating: (189)
|
Hi, As far as I'm aware, to get your 3rd party points into a PXC4, you need to add them manually into the PXC4. As an example, to read an 3rd party analog point - add an R_A block into the PXC4. Once the basic points are added, you then need to address the PX points appropriately to link them to the 3rd party points (i.e. configure the Device Instance number; the Object Type code; and the Object Instance number). There's a video link HERE where you can get some more information. Although the video refers to mapping points from devices within ABT, the concept is still explained as to where to address your 3rd party points - refer to time stamp 01:36 and onwards in the video. This shows where the addressing info is set. Regards, |
Last edited by: Jen_Moderator at: 01/19/2022 09:35:49Embedded video. |
|
1/24/2022 10:53 PM | |
Joined: 8/17/2021 Last visit: 9/27/2024 Posts: 200 Rating: (3) |
Thank you |
This contribution was helpful to1 thankful Users |
Follow us on