5/16/2022 9:28 AM | |
Joined: 3/11/2019 Last visit: 7/9/2024 Posts: 1511 Rating:
|
Dear Roby,
It is possible. Can you ping the device AND the cpu at the same time (from same network)? But also a IP or PROFINET device name missmatch can be a reason..... Is the online diagnostics of the device accessible (with TIA)? Information to symbol can be found here: Displaying diagnostics status and comparison status using icons-> table for diagnostic icons -> "The module or the device cannot be reached from the CPU (valid for modules and devices below a CPU)." regards sancruz |
Feedback appreciated, please rate |
|
This contribution was helpful to
2 thankful Users |
Follow us on