3/23/2022 11:59 AM | |
Joined: 9/21/2015 Last visit: 7/2/2024 Posts: 6 Rating:
|
Hello, I'm experiencing the same issue in a system: I have in TIA V14 SP1 several PLC 1214C Fw V4.2.2 equipped with CP 1243-1 Fw 3.0.23; as soon I have set in the CP the time synchronization via NTP (the server is a Windows PC) I got random hardware configuration errors caused by CP, that resulting in CPU STOP. I have several devices with this PLC configuration and this problem is affecting almost 50% of devices and it's occuring more or less every 30-40 days. Has anyone any solution about this issue? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/23/2022 12:48:24New subject after splitting |
|
Follow us on