8/30/2023 7:54 AM | |
Joined: 4/18/2023 Last visit: 9/21/2023 Posts: 1 Rating:
|
One Line description in issue – Drive manufacturer alarms/warning not displayed in PLC Diagnostic buffer in S7-300 CPU and same Drive manufacturer alarms/warning displayed in S71200 and S7-1500 PLC. Details Description - 2. In Danfoss Drives alarm generated and arenot ableto view manufacturer alarm details is S7-300(CPU315-2PN/DP)PLC diagnostic buffer and the same Drive connected with S7-1200 (CPU 1214 DC/DC/DC) PLC with Profibus communication CM 1243-5 (6GK7 243-5DX30-0XE0) and S7-1500 (CPU1516F-3 PN/DP) can see manufacturer alarms/warnings in PLC diagnostic buffer. attached images for S7-300/1200/1500 PLC Diagnostic Buffer. 3. After analyzing the ProfiTrace logs, I was able to see that Drive sent the same message to the S7-1200, S7-1500 PLC and the S7-300 PLC. I have attached logs image. (ProfiTrace_logs S7-300 and S7-1200) AttachmentProfiTrace_logs S7-300 and S7-1200.zip (105 Downloads) |
Follow us on