11/2/2023 8:12 PM | |
Joined: 5/15/2023 Last visit: 12/26/2023 Posts: 19 Rating: (0) |
Hello. Yes, we checked, there is a connection and the data is present, We wrote a program and added blocks. There are no errors in the project. but I don't get the data from the weight cell ------------------------------------------------------------------------------------------ AttachmentTD_CFI_TIADemo_V1.0_EN.pdf (270 Downloads) |
Last edited by: Jen_Moderator at: 11/16/2023 09:18:23Copy of the post created for better understanding and to attach the file. Splitting remark embedded. |
|
11/15/2023 9:42 AM | |
Joined: 4/28/2015 Last visit: 2/7/2024 Posts: 10533 Rating: (819) |
Hello, all this problematic is more bigger than we can expect because Wipotec offers also this kind of gateway as required inter component that connects all CAN devices to expected fieldbus system. Wipotec CAN Gateway (Wipotec web) Really I understand probably that you have bypassed this Gateway probably and you have idea to connect on CAN bus with that weigh cell attached but this is that hard work to do, set correctly this weigh cell on CAN bus to have proper data from it to your higher system. Here is required manual to this cell where data are concentrated (Index,...) and also with Wago SW where you need configure your 658 module with that required data from cell manual. Really I don't know if some one here will help you further in this cfg. I'm able maybe continue with help and tips but pls also understand that I don't have your HW and is simply impossible to give exact help. Again pls what is important to know, what exactly HW cfg you have now and what SW solution you did till this time? I'm also curious who from your place have selected this solution as Wago 658 and other things? Very sry but it looks to me that you have not. |
Last edited by: Duris_I at: 11/15/2023 09:45:08Last edited by: Duris_I at: 11/15/2023 09:48:06With best regards... |
|
Follow us on