7/13/2024 7:58 AM | |
Joined: 6/28/2024 Last visit: 7/13/2024 Posts: 3 Rating:
|
Hi everyone, I'm having issue in converting the VBscript from my previous Comfort HMI project to the HMI script that will be used in WinCC Unified. The script that worked in "Comfort" is not working in WinCC Unified. FYI, the JS script used in the WinCC Unified are the script I converted from the VBscript (attached in zip) with reference to the script converted using ChatGPT. The JS script used have no syntax error and I'm confused where did I go wrong or miss. Hoping to get help from everyone. Thanks. With Regards. AttachmentVBscript to Unified.zip (0 Downloads) |
Follow us on