8/10/2024 6:54 AM | |
Joined: 12/18/2014 Last visit: 10/17/2024 Posts: 33978 Rating: (4224)
|
Who set M1 to high? A remote device? |
8/10/2024 8:05 AM | |
Joined: 8/2/2024 Last visit: 8/12/2024 Posts: 11 Rating: (0) |
That's right. I use Modbus TCP and send the value 1 to M1 using Modbus Poll. |
8/10/2024 10:46 AM | |
Joined: 12/18/2014 Last visit: 10/17/2024 Posts: 33978 Rating: (4224)
|
It's the problem as in this topic? make PLC retain the last value it read from the slave |
8/12/2024 5:15 AM | |
Joined: 9/11/2014 Last visit: 10/17/2024 Posts: 770 Rating: (31) |
Hi, a LOGO! 8.4 has an additional retentive memory rage (VRx). This can be used to solve such RQ. |
8/12/2024 3:20 PM | |
Joined: 12/18/2014 Last visit: 10/17/2024 Posts: 33978 Rating: (4224)
|
I see it the same way as the user gwazee. I carried out a small test. To do this, I transferred the MB0 of a remote LOGO! to the VRB0 of the LOGO! 8.4. What is the point of the remanence then? AttachmentScreencast 2024-08-12 16-36-23.zip (169 Downloads) |
Last edited by: ixo65 at: 08/12/2024 15:21:44 |
|
Follow us on