10/16/2024 7:03 AM | |
Joined: 3/11/2019 Last visit: 11/8/2024 Posts: 1653 Rating: (304) |
Hi, in general you can try a repair installation of V5.7 via the windows control panel for the apps and features, sometimes this can help. Otherwise check if the latest version von V5.7 + servicepacks + hotfixes is used. Should be V5.7 + servicepack 2 + hotfix 1 (may someone correct me, if I am wrong). SIMATIC STEP 7 V5.7 SP2 Trial Download
Download Hotfix 1 STEP 7 V5.7 SP2 / STEP 7 Professional 2021 SR2regards sancruz |
Feedback appreciated, please rate |
|
This contribution was helpful to1 thankful Users |
10/16/2024 8:51 AM | |
Joined: 3/11/2019 Last visit: 11/8/2024 Posts: 1653 Rating: (304) |
Hi, thank you for your feedback. If you want to be sure, I would suggest to create a Support Request. We volunteers may have some personal experience if someone run into the same issue, but besides that not really any details. regards sancruz |
Feedback appreciated, please rate |
|
Follow us on