6/22/2006 5:40 PM | |
Joined: 8/31/2005 Last visit: 6/14/2024 Posts: 2198 Rating: (328) |
[quote user="muneeb"]Can anyone inform me that whether the S7 software matches with the following international standards? 1. NEMA IA 2.3 & 2.3(IEC 61131,parts-2&3) 2. UL 508,part XVII 3. ANSI/IEEE C37.90.1 4. IEC 61131 In the support pages you can find 7 Approvals/Certificates or SIMATIC S7 Software: http://support.automation.siemens.com/WW/view/en/10805382/134200 and138 forSIMATIC S7 Hardware: http://support.automation.siemens.com/WW/view/en/10805148/134200 |
Last edited by: miami at: 6/22/2006 5:40 PM |
|
Follow us on