2/3/2011 10:57 AM | |
Posts: 4 Rating: (0) |
Hi friends, [schnippschnapp] I have siemens c7 635key.The process is controlled with the the s7 program written in the integrated CPU.If I switch over the TP mode to Transfer mode for Complete Back Up using Prosave,will the CPU also go to stop mode?Without going to Transfer mode can I do Back up? Please help me in clearing my doubts. Regards, Friend Splitted from downloading to OP170B. |
Last edited by: O_Moderator at: 2/3/2011 12:57 PMnew subject after splitting |
|
Follow us on