3/14/2011 9:59 AM | |
Posts: 6 Rating: (0) |
Dear all, i heard that: you could simu more than one PLC in the PLCSim for testing communication ( Master/Slave; Profibus-DP...), but i can open 2 or more PLC in PLCSim. So please tell me the way i can do that or explain to me why no? and if you have an example about testing communication bewteen 2 PLC, please upload it here. Thanks much, Splitted from If I use two CPUs for two different machines, can the CPUs share one HMI, like the KTP600?. |
Last edited by: O_Moderator at: 3/14/2011 10:20 AMnew subject after splitting. contact data deleted |
|
3/14/2011 10:58 AM | |
Posts: 316 Rating: (37) |
Hi, until the PLCSIM V5.4 SP3 the new function new functions "Multiple startability (multi-instance capability) and communication support between the simulated CPUs (simulation instance)" will be provided. More information: PLCSIM V5.4 SP3 If you want the newest SP --> PLCSIM V5.4 SP4 An example you can find on this link: http://support.automation.siemens.com/WW/view/en/38726591 |
Follow us on